AOUT#.OFFSET
Description
This parameter sets the analog output offset.
Examples
Code
--> AOUT2.VALUEU 5 --> AOUT2.VALUE 5.000 V --> AOUT2.OFFSET -1 --> AOUT2.VALUE 4.000 V --> AOUT2.VALUEU 5.000 V
Context
For more information see Analog Output.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | V |
| Range | -10V to +10V |
| Default Value | 0 V |
| Data Type | Float |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.